SDK 6.3 Hall Initialization Failing and Missing mp_hall_tuning.c File
I'm working on a project with the EVALSTDRIVE101, and my motor has Hall sensors. I'm able to use the Hall sensors with SDK 6.2, but with SDK 6.3, the processor runs to the HardFault_Handler routine if the Hall sensors are enabled (as an auxiliary speed sensor).
If the Hall sensor is enabled, the HT_Init function is called in the FOC_Init function in the mc_tasks_foc.c file. However, if I step into the function, a file opens indicating "Can't find a source file ... mp_hall_tuning.c." If I keep stepping through the disassembly, I eventually get to the fault routine. Something obviously broke in the new implementation.
Can someone tell me where the mp_hall_tuning.c file is and why I don't have access to it? Is it included in a precompiled statically compiled library or something?