Sensorless BLDC Motor Issues Using Nucleo-F401RE and X-NUCLEO-IHM16M1
Dear ST Team,
I am currently working on a 24V @ 1.5A sensorless BLDC motor control application using the following setup:
- MCU Board: Nucleo-F401RE
- Driver Board: X-NUCLEO-IHM16M1
- Motor: Sensorless BLDC Motor
- Software Tools: MC Workbench 6.4.0 and Motor Pilot
- Control Technique: Field-Oriented Control (Sensorless)
Issues Observed:
- During startup, the motor produces loud noise, initial jerks, and fault indications in the IHM16M1 board.
- At higher RPMs, a mild humming noise is audible.
- When decreasing the speed to medium or lower RPMs, the IHM16M1 board triggers faults again in the IHM16M1 board.
We have profiled the motor multiple times using Motor Pilot, and each profiling run gave slightly different values for parameters such as Friction, Inertia, and Back-EMF constant.
To address this, we tested the system using the average, minimum, and maximum values obtained from multiple profiles. However, the same issues persisted across all tests — specifically during startup, low-speed operation, and at maximum speed.
We’ve attached a profiling table for your reference
Max Current | R(ohm) | L(mH) | K(Vrms/kRPM) | F(uN.m.s) | Inertia(uN.m.s2) | Max RPM |
1.2 | 1.58 | 1.24 | 26.33 | 753.61 | 22608.98 | 306 |
1.2 | 1.59 | 1.25 | 26.93 | 937.67 | 28131.12 | 312 |
1.3 | 1.59 | 1.26 | 27 | 1242.01 | 37261.63 | 330 |
1.3 | 1.6 | 1.27 | 28.61 | 1339.53 | 40187.38 | 336 |
1.35 | 1.6 | 1.28 | 28.76 | 1497.54 | 44927.62 | 348 |
1.4 | 1.6 | 1.22 | 32.05 | 965.57 | 28967.94 | 324 |
1.4 | 1.61 | 1.23 | 32.3 | 1422 | 42661.48 | 330 |
1.4 | 1.6 | 1.21 | 29.03 | 754.78 | 22644.21 | 336 |
1.4 | 1.61 | 1.28 | 31.05 | 1050.73 | 31523.09 | 336 |
1.4 | 1.62 | 1.22 | 26.66 | 1198.17 | 25946.32 | 354 |
1.4 | 1.62 | 1.21 | 28.96 | 879.03 | 26371.63 | 336 |
Table 1
Request for Support:
- How can we reduce startup jerks and noise?
- Is there any detailed guidance on how to tune the rev-up control table and observer settings for sensorless operation?
- How can we stabilize the motor at lower RPMs to avoid fault generation in the IHM16M1 board?
- Is there a way to reduce humming noise at higher RPMs?
Any documentation, configuration guidance, or tuning tips specific to IHM16M1 and F401RE with sensorless FOC control would be highly appreciated.
Thank you in advance for your support.
Best regards,
Rahul