Shunt resistor value differency between Motor Control Workbench/source code and user manual.
I'm trying to control a PMSM motor using Nucleo-G474RE and STEVAL-IHM023V3 motor control boards and Motor Control WorkBench (Version 6.2.1).
I have noticed that the values of shunt resistors (R55, R68, and R101) are given as 150 mOhm in User Manual UM1823 (pages 13, 14, 15) while 100 mOhm in source code (power_stage_parameter.h, line 46) and Motor Control Workbench software. I have visually inspected the STEVAL-IHM023V3 motor control board and seen that shunt resistors' values are 150 mOhm.
The PMSM motor is rotating normally when I create, compile and run the source code via Motor Control WorkBench (for default 100 mOhm shunt resistor value in the Motor Control Workbench).
But when i changed the RSHUNT value at the power_stage_parameter.h, line 46 to 150 mOhm, PMSM motor started to rotate abnormally.
Can someone explain to me the value differency between the source code and the user manual for the shunt resistors R55, R68 and R101? Am i missing a point?