Skip to main content
Associate II
August 1, 2023
Solved

ST Evaluation Board EVSPIN32G4

  • August 1, 2023
  • 1 reply
  • 1273 views
Hi 
 
 i have recently purchased for ST Evaluation Board EVSPIN32G4 
 
 
Supply voltage Nominal From 10 V to 75 V

Maximum output current with heatsink (EVSPIN32G4) Peak 35 A
Continuous(1)  20 Arms 
Maximum output current without heatsink (EVSPIN32G4NH) Peak 25 A
Continuous(1)  15 Arms 
 
 Output Vaiable Volt AC OR DC ? and frequency Range How much?  
 
Regards
kumar Raja 
coimbatore
    This topic has been closed for replies.
    Best answer by MMenz.1

    Hi Kumar,

    Not sure what you mean with output voltage. The FET connect the DC supply voltage to the Motor, so the maximum voltage with a PWM dutycycle of 100% is the DC supply voltage.

    The switching frequency can be set in the MC Workbench from 2 to 100kHz but is 30kHz by default.

    1 reply

    GMA
    Technical Moderator
    September 14, 2023

    Dear Kumar Raja,

    Firstly, we would like to sincerely apologize for the delay in replying to your post.
    If your point is still pertinent, you can find the full documentation set here: EVSPIN32G4.
    The maximum MCU frequency is 170Mhz.
    The allowed DC supply voltage is from 10V to 75V.


    If you agree with the answer, please accept it by clicking on 'Accept as solution'.Best regards.GMA
    Associate II
    January 6, 2024

    Hi.,

    EVSPIN32G4

    I am asking only for output Voltage (switching variable voltage ac or dc ) and output switching frequency.

    warm Regards

    Kumar Raja

    MMenz.1
    MMenz.1Best answer
    Associate II
    January 10, 2024

    Hi Kumar,

    Not sure what you mean with output voltage. The FET connect the DC supply voltage to the Motor, so the maximum voltage with a PWM dutycycle of 100% is the DC supply voltage.

    The switching frequency can be set in the MC Workbench from 2 to 100kHz but is 30kHz by default.