Skip to main content
Kamil1
Associate II
January 7, 2025
Solved

Steval esc001v1 UART pin order

  • January 7, 2025
  • 1 reply
  • 702 views

Hello, could someone please advise me what is the correct order of the UART pins on the steval esc001v1.

 

thank you

 

Kamil

uart pins 4321uart pins 4321uart pins 1234uart pins 1234from esc manualfrom esc manual

Best answer by Andrew Neil

Do you have the board? Is there an ident marked on it?

It looks like there might be  but, in the photo, it's obscured by the capacitor:

AndrewNeil_0-1736274632511.png

 

Failing that, look at the Gerbers and/or CAD files: see which pin is GND - you can get the rest from that

1 reply

Andrew Neil
Super User
January 7, 2025
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Kamil1
Kamil1Author
Associate II
January 7, 2025

Thank you for quick answer, however I need to know if the pin no.1 is closest to the capacitor or the oposite one.  

 

Kamil

Andrew Neil
Andrew NeilBest answer
Super User
January 7, 2025

Do you have the board? Is there an ident marked on it?

It looks like there might be  but, in the photo, it's obscured by the capacitor:

AndrewNeil_0-1736274632511.png

 

Failing that, look at the Gerbers and/or CAD files: see which pin is GND - you can get the rest from that

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.