STM32 IHM07M1 STM32F401RE Motor profiler
Hello,
Did anyone attempt to use the motor profiler toolkit with these boards : STM32 IHM07M1 & STM32F401RE? I configured mine following the "motor control mode" from ST website and the program starts but then nothing happens and the following error message appears : "The measurement is taking too time".
On the other hand if I use the motor pilot tool with some approximate motor parameters, everything woks fine, so I think the problem comes from the indications on how to configure the board in the beginning for the profiler.
Any help would be largely appreciated! Thanks a lot in advance
Florian