Skip to main content
Associate
November 28, 2024
Question

STSPIN32G4 EMI radiation problem

  • November 28, 2024
  • 0 replies
  • 425 views

Hello I need help for STSPIN32G4 EMI Issue

I took tests for Farfield EMI Report at STSPIN32G4 Standby condition
Report shows QP are over than Limit at 189 MHz, 252MHz.  It doesnt depend on the input voltage and the signal  peeks are visible also if the microcontroler is running in the loop only.

Similar problem has also another user Dkim-39 and here is his measurement.  Do you have any solution for this problem?

Thanks   Josef Pazderka

 

jopa_0-1732780186721.png