Support for MCSDK for STM32H747XIH6
We have an application where we need to use the STM32H747XI with it's MIPI DSI display and the corresponding application running on CM7 and we need to commutate a BLDC motor on with the CM4. There is support for NUCLEOH745ZI on on the STM32CubeMX but we need to implement it on the STM32H747XI. I tried to port the whole middleware of MotorControl to it but I'm unable to complete my requirement. Is there anyway of acquiring native support for STM32H747I-DISCO for the MCSDK, I have little experience with the STM32 environment.