Synch TIMs on G0B1RE
Hello,
I'm working with the NUCLEO-G0B1RE, controlling some motors.
In order to correctly control motor I need to synchronize to timers. For this, I chose to use TIM3 and TIM15 TIM15 on Slave-Gated mode
My issue is that when the TIM3 and TIM15 start running they have nearly, but not the same, CNT.
However, after some time the TIM3 and TIM15 are clearly not synch. They seem to follow each other but with a difference of ~700 ticks.
Clock Tree is not the same for both Timers, but the frequency is configured to be the same.
I attach some print screens of the configuration. I can post completly the code, or clock tree...etc. if required.
Thank you for your help!