Solved
Troubleshooting of STEVAL-IHM028V2
- November 19, 2024
- 1 reply
- 1924 views
Hello,
While I did tests with my motor control STEVAL-IHM028V2, I made a mistake to schort-circuit the three-phase output ! Then, I smelled a burning smell and no voltage is given in the three-phase output . When I checked the bottom face of the device, I noticed that some resistors (R74, R75 and R69) are burned (see attached images). Also, the W7 and W8 jumpers are short-cicuited. How could I fix this issue ?
N.B. The schematic of the STEVAL-IHM028V2 is attached.
Cordially
Tarek