UART communication between ST MotorPilot and STEVAL-SPIN3202
Hi ST,
I am unable to establish UART communication between ST MotorPilot and STEVAL-SPIN3202.
I am uploading one of the two STEVAL-SPIN3202 examples.
Setting up 9600 baud rate (same as in Cube MX settings). Using correct COM port.
Hardware setup:
Power 24VDC connected.
USB connected.
J9: OPEN (BOOT0). (closing does not do any change)
J7: OPEN.
If I debug it:
and resume,
I observe green/red USB LEDs blinking.
I am trying to connect with ST MotorPilot - result:
If I run it:

it does not blink red/green USB LEDS and result is the same, no matter whether If close J9 or not and reset the MCU.
Result is the same, :
What am I doing wrong?
Should I Run or Debug?
Regards,
Edward.