Unexpected OPAMP Output Voltage When Enabling OPAMP on EVSPIN32G4 DUAL
I am using EVSPIN32G4 DUAL and observed the following behavior.
When calling:
LL_OPAMP_Enable(OPAMPx);
the OPAMP output immediately shows about 208 mV.
I measured this voltage at TP25.

This behavior occurs even though DAC3 is completely disabled.
After calling LL_OPAMP_Enable(), I checked the DAC3 registers and confirmed that:

All related DAC_CR and DAC_DHR12R registers remain set to zero.
I checked these registers because DAC3 Channel 2 is configured as the OPAMP minus (−) input, as shown in the configuration below.

My questions are:
1. Why does the OPAMP output show approximately 208 mV when the OPAMP is enabled ,even though DAC3 has no value configured and is fully disabled?
Thank you.
Best regards,
Pelino