VNH5019 Current sense gain accuracy/tolerance
I was looking at the datasheet for the VNH5019, and saw that the current sense gain tolerance is narrower as it drives higher currents. I am trying to use the driver in an application where the motor currents can range from about 100mA to 10 A, and am hoping to gain some insight on the tolerance range for the current sense in the 0 - 1000mA range, since I have seen a very wide range of errors in the current sense calculation (up to 100%, with outliers even worse than that).