Skip to main content
MKoms.2
Visitor II
March 13, 2023
Question

"Warning! Hardware changes must be applied to the following signals" meaning

  • March 13, 2023
  • 2 replies
  • 1399 views

Hi,

I am working on a motor control application and created my project based on X-NUCLEO-IHM08M1 + NUCLEO-F302R8. I observed an warning in MC workbench saying:

Warning! Hardware changes must be applied to the following signals. Please, refer to the board diagram for details.

PA0 CURRENT_AMPL_U

PC1 CURRENT_AMPL_V

PC0 CURRENT_AMPL_W

what does this exactly mean? What should I do to get them removed.

This topic has been closed for replies.

2 replies

cedric H
Technical Moderator
March 23, 2023

Hello @MKoms.2​ ,

The ST boards are configurable and can be used for Single Shunt, Three Shunt FOC or 6 steps.

This message is just there to warn you that a small modification has to be done on the board to match your selected configuration. We plan to improve this message in the next release, and a way to acknowledge it.

Regards

Cedric.

Explorer II
September 1, 2023

Moving response to reply to OP.

Explorer II
September 1, 2023

@MKoms.2 wrote:

Hi,

 

I am working on a motor control application and created my project based on X-NUCLEO-IHM08M1 + NUCLEO-F302R8. I observed an warning in MC workbench saying:

 

Warning! Hardware changes must be applied to the following signals. Please, refer to the board diagram for details.

 

PA0 CURRENT_AMPL_U

PC1 CURRENT_AMPL_V

PC0 CURRENT_AMPL_W

 

what does this exactly mean? What should I do to get them removed.


It's been a few montsh since OP's post so I'm assuming they got past it. For anyone else that might get this message, just generate the code then fix the pin assignments in CubeMX as needed for your application.