Skip to main content
DMeie.2
Associate III
May 16, 2024
Question

What are the maximum motor electrical parameters?

  • May 16, 2024
  • 0 replies
  • 522 views

What's the maximum/minimum electrical parameters for the motors that can be used with the MCSDK?
Especially the important parameters like winding inductance and resistance values.

We're trying to get a motor to run that has a Stator Resistance of 0.011Ohms and an inductance of 8.1µH@1000Hz (manufacturer datasheet), so the values in the motor json are "rs": 0.011 and "ls": 0.0081.

This topic has been closed for replies.