Which power board should I choose?
Hi,
I want to control a PMSM using STM32 FOC SDK.
And the spec of the PMSM is below
Rated input volt: 62 V
Rated current: 2.5 A
Rated output: 200W
But I notice the voltage sets of power broad are
10~28 Vdc
8~48 Vdc
125~400 Vdc
could I choose 8~48 Vdc range to control my PMSM?
Like X-NUCLEO-IHM08M1 power board.
(But the motor speed may slower than the value on datasheet)
Or should I follow the Watt?
Like STEVAL-IPM05F (500W power board).
(But I am not sure the output voltage will under 62V or not)