Which ST control board should I choose to detect motor parameters?
Hello Everybody,
I have a high-power BLDC motor with a rated power of 200W and a nominal voltage of 24V, resulting in a current draw of approximately 10A. I intend to use Motor Profiler to detect detailed motor parameters (e.g., B-EMF constant). Could you advise on which ST control board is suitable? I know there are many control boards like NUCLEO-G431RB. Given the high current, is the control board with the Three-Shunt current sensing inappropriate? If so, what alternative control board should I select? Thank you!