Solved
Why I_Q_MEAS is zero when motor is locked and I_Q_REF goes up to the maximum value?
- March 31, 2024
- 1 reply
- 1346 views
I'm using ST workbench 6.2.0 and motor Pilot V1.2.4. NUCLEO+ IHM08M1, three shunt sensor and brushless motor with encoder.
When the motor is blocked, using TORQUE control-->Torque Ramp in Motor Pilot, the actual drive current I_Q_MEAS is almost zero, although the Torque_Reference and I_Q_REF is shown to reach the expected value.
Once the motor is unblocked, everything seems to be fine.
It seems to me that since the actual Iq is almost zero, the drive isn't capable of delivering maximum starting torque.
What am I missing here?