X-NUCLEO-IHM07M1 with NUCLEO-F446RE Not Spinning A2212-13T BLDC Motor
Hi,
I'm working on a BLDC motor control project using the X-NUCLEO-IHM07M1 driver board with a NUCLEO-F446RE. I'm trying to control an A2212-13T BLDC motor (1000KV) with a 12V power supply at 2.5A, and targeting around 5000 RPM, but the motor does not spin at all.
I have confirmed that the jumper settings on the X-NUCLEO-IHM07M1 are set correctly for 3-shunt operation, and the firmware is properly loaded using STM's MCSDK.
However, when I use the same motor and power conditions with the B-G431B-ESC1 board, the motor spins as expected.
While searching the STM Community, I found several similar issues reported when users try to run motors other than the Bull Running BR2804-1700KV (used in STM’s tutorial videos). Unfortunately, most of those threads have no final solution.
Is there something about the IHM07M1 or the motor parameter configuration that causes compatibility issues with common hobby BLDC motors like the A2212?
Any advice or working configuration examples would be appreciated.
Thanks!