X-Nucleo-IHM17M1 and NUCLEO-F303RE 3 Shunt topology
Good day,
I'm trying to get motor profiler running on an X-Nucleo-IHM17M1. The only compatible Nucleo board I have is a F303RE.
To enable the motor profiler application, it requires the selection of 3 shunt current sensing. According to this link, it seems that both the IHM17M1 and F303RE support 3 shunt current sensing.

Yet, when I try and configure the project, only single shunt is available. This is not the case for the other Nucleo boards.

That said, I do receive the following warning when creating the project.

Is there any solution for this, or should I use a different Nulceo board?