Skip to main content
Visitor II
January 20, 2026
Question

ADC not working with PCLK / 4 ?

  • January 20, 2026
  • 1 reply
  • 146 views

Hi,

 

Im using STM32g0b1 ADC in continous mode.

I am continously converting channels 0,1 and 2. Everything works perfect when clocking the ADC with PCLK/2.

SYSCLOCK is 64MHz

PCLK is 64MHz

 so ADCCLOCK is 32MHz.

I get End-of-Conversion Interrupts correctly and each 3rd EOC interrupt I am getting an End-of Sequence interrupt.

 

If I use PCLK/4 (ADCCLOCK 16MHz)  the timing for conversions is seemingly as intended (everything takes exactly double time), however channels get mixed.

I found that End-of Sequence interrupt occurs every two conversion (instead of every three conversion) and I can no longer match Conversion results to channels.

In fact channel 2 conversion result ends up as first, second or third result within a series.

 

Remark: I started to check for End-of Sequence interrupt only after getting above problem.

 

Is there restriction about clocking the ADC?

 

 

 

 

 

1 reply

TDK
Super User
January 20, 2026

There's no restriction on the ADC clock. There's probably a bug in your code.

"If you feel a post has answered your question, please click ""Accept as Solution""."