Skip to main content
Visitor II
September 15, 2025
Solved

CAN Loopback Test using STM32 NUCLEO-L452RE

  • September 15, 2025
  • 2 replies
  • 386 views

It seems like the program is getting stuck in the Error_Handler loop and not coming out. Could there be a problem with my code?

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2025 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "can.h"
#include "usart.h"
#include "gpio.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */

/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/

/* USER CODE BEGIN PV */
CAN_TxHeaderTypeDef TxHeader;
CAN_RxHeaderTypeDef RxHeader;
uint8_t TxData[8];
uint8_t RxData[8];
uint32_t TxMailbox;
uint8_t button_pressed_flag = 0;
uint8_t message_received_flag = 0;

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_USART2_UART_Init();
 MX_CAN1_Init();
 /* USER CODE BEGIN 2 */
 // 1. CAN 수신 필터 설정 (Loopback에서도 필수는 동일)
 CAN_FilterTypeDef canfilterconfig;
 canfilterconfig.FilterActivation = CAN_FILTER_ENABLE;
 canfilterconfig.FilterBank = 0;
 canfilterconfig.FilterFIFOAssignment = CAN_RX_FIFO0;
 canfilterconfig.FilterIdHigh = 0x0000;
 canfilterconfig.FilterIdLow = 0x0000;
 canfilterconfig.FilterMaskIdHigh = 0x0000;
 canfilterconfig.FilterMaskIdLow = 0x0000;
 canfilterconfig.FilterMode = CAN_FILTERMODE_IDMASK;
 canfilterconfig.FilterScale = CAN_FILTERSCALE_32BIT;

 if (HAL_CAN_ConfigFilter(&hcan1, &canfilterconfig) != HAL_OK)
 {
 Error_Handler();
 }

 // 2. CAN 통신 시작
 if (HAL_CAN_Start(&hcan1) != HAL_OK)
 {
 Error_Handler();
 }

 // 3. CAN 수신 메시지 알림(인터럽트) 활성화
 if (HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO0_MSG_PENDING) != HAL_OK)
 {
 Error_Handler();
 }

 // 4. 전송할 메시지 헤더 기본 설정
 TxHeader.IDE = CAN_ID_STD;
 TxHeader.StdId = 0x123; // 메시지 ID
 TxHeader.RTR = CAN_RTR_DATA;
 TxHeader.DLC = 1; // 데이터 길이 (1바이트)
 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
	 // 1. 버튼이 눌렸으면 메시지 전송
	 if (button_pressed_flag == 1)
	 {
	 button_pressed_flag = 0; // 플래그 초기화

	 TxData[0]++; // 보낼 때마다 데이터 1씩 증가

	 if (HAL_CAN_AddTxMessage(&hcan1, &TxHeader, TxData, &TxMailbox) != HAL_OK)
	 {
	 Error_Handler();
	 }
	 }

	 // 2. 메시지가 수신되었으면 LED 토글
	 if (message_received_flag == 1)
	 {
	 message_received_flag = 0; // 플래그 초기화
	 HAL_GPIO_TogglePin(LD2_GPIO_Port, LD2_Pin); // 녹색 LED 깜빡이기
	 }
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */


 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Configure the main internal regulator output voltage
 */
 if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.HSICalibrationValue = 64;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
 RCC_OscInitStruct.PLL.PLLM = 1;
 RCC_OscInitStruct.PLL.PLLN = 10;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV7;
 RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2;
 RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) != HAL_OK)
 {
 Error_Handler();
 }
}

/* USER CODE BEGIN 4 */
/**
 * @brief CAN 메시지 수신 완료 시 호출되는 콜백 함수
 */
void HAL_CAN_RxFifo0MsgPendingCallback(CAN_HandleTypeDef *hcan)
{
 if (HAL_CAN_GetRxMessage(hcan, CAN_RX_FIFO0, &RxHeader, RxData) == HAL_OK)
 {
 // 수신된 ID가 내가 보낸 ID와 일치하는지 확인
 if (RxHeader.StdId == 0x123)
 {
 message_received_flag = 1; // 수신 플래그 설정
 }
 }
}
/**
 * @brief 외부 인터럽트(버튼) 발생 시 호출되는 콜백 함수
 */
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
 if (GPIO_Pin == B1_Pin)
 {
 button_pressed_flag = 1; // 버튼 플래그 설정
 }
}
/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
	 // 오류 발생 시 녹색 LED가 매우 빠르게 깜빡이도록 설정
	 HAL_GPIO_TogglePin(LD2_GPIO_Port, LD2_Pin);
	 HAL_Delay(100);
 }
 /* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * file: pointer to the source file name
 * line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
Best answer by Karl Yamashita

Some code are missing that typically are produced by CubeMX or STM32CubeIDE

 

/* Private variables ---------------------------------------------------------*/
CAN_HandleTypeDef hcan1; // You're missing this

/* USER CODE BEGIN PV */

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);// You're missing this
static void MX_CAN1_Init(void);// You're missing this
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

 

Not sure how you're getting the project to build, if hcan1 is not defined?

Are you copying code from somewhere or did you use CubeMX/STM32CubeIDE to generate the code?

2 replies

mƎALLEm
Technical Moderator
September 15, 2025

Hello @OH_it and welcome to the St community,

You didn't share the CAN configuration? The GPIOs configuration of Tx/Rx? and you didn't tell on which Error_Handler() it was stuck? which line?

You can also refer to this article: Guide to CAN (bxCAN/CAN2.0) configuration in Loop back mode on STM32 MCUs

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
Karl Yamashita
Karl YamashitaBest answer
Principal
September 15, 2025

Some code are missing that typically are produced by CubeMX or STM32CubeIDE

 

/* Private variables ---------------------------------------------------------*/
CAN_HandleTypeDef hcan1; // You're missing this

/* USER CODE BEGIN PV */

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);// You're missing this
static void MX_CAN1_Init(void);// You're missing this
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

 

Not sure how you're getting the project to build, if hcan1 is not defined?

Are you copying code from somewhere or did you use CubeMX/STM32CubeIDE to generate the code?

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source