Designing a custom board with STM32H725ZGT3
- July 30, 2025
- 4 replies
- 362 views
I designed a custom board using the STM32H725ZGT3. The references I followed include the datasheet, application note AN5419, and the STM32H745ZIT6 Nucleo board design, among others.
After powering up the board, I was able to connect to it via ST-Link using STM32CubeProgrammer, and successfully uploaded a simple blink code using STM32CubeIDE. The code worked, and the LED started blinking.
However, after a power cycle (i.e., turning the main power off and on again), the board stopped running the code, and the LED no longer blinked. I tried reconnecting with STM32CubeProgrammer, but I received a "Target not found" error.
After that, I connected the BOOT pin to 3.3V. This allowed me to connect to the board again using STM32CubeProgrammer, but I couldn’t upload code using STM32CubeIDE. I then changed a setting in the CubeIDE:
System Core → RCC → Parameter Settings → Power Parameters → PWR_LDO_SUPPLY
After this change, I was able to successfully upload the code. However, the LED no longer blinked as before. I tried connecting the BOOT pin to ground again, but it still didn’t work.
My Questions:
Is my schematic correct?
Is the MCU damaged?
If the code uploads successfully and the board connects, why is the LED not blinking? Could it
be a power issue?