Skip to main content
Associate II
September 7, 2025
Solved

Does STM32H750 support mem2mem DMA (ChatGPT said it doesn't)?

  • September 7, 2025
  • 3 replies
  • 422 views

Hi Dear friends,

 

I am trying to configure H750 to transfer data between internal SRAM and external SDRAM, I got everything setup OK but with some problems (also monitor data bus with logic analyzer). So I checked with ChatGPT, surprisingly, ChatGPT said H750 (actually it said the same thing about H74x)  does not officially support memory-to-memory transfer, ChatGPR said use MDMA instead. Before I jump into MDMA, just want to make sure what ChatGPT said is true?

 

Thanks.

 

 

Best answer by mƎALLEm

Hello,

From the reference manual / table 3:

mALLEm_0-1757322323479.png

So you can do transfers from/to SRAM1/SRAM2/SRAM3 <-> FMC. you cannot do that transfer to from DTCM/ITCM. You need MDMA for that.

BDMA could not do that kind of transfer.

3 replies

TDK
Super User
September 7, 2025

What does the Reference Manual say?

"If you feel a post has answered your question, please click ""Accept as Solution""."
yah1003Author
Associate II
September 7, 2025

Hi,

 

Reference Manual does not say any thing about this (at least not that I could find), it just gives a general description not specifically for SDRAM<->SRAM 

Pavel A.
Super User
September 7, 2025

Hi,

For H750 please see the bus matrix picture in RM0433

The full story is a bit complicated. Chatgpt can elaborate more.

 

yah1003Author
Associate II
September 8, 2025

Yes, I already checked the reference manual for the DMA, but don't know what I should look for, I've spent a whole day trying it on real hardware and it seems DMA between SDRAM and SRAM works, but that is just for very limited test I've done! Could you elaborate more?

mƎALLEm
mƎALLEmBest answer
Technical Moderator
September 8, 2025

Hello,

From the reference manual / table 3:

mALLEm_0-1757322323479.png

So you can do transfers from/to SRAM1/SRAM2/SRAM3 <-> FMC. you cannot do that transfer to from DTCM/ITCM. You need MDMA for that.

BDMA could not do that kind of transfer.

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
Pavel A.
Super User
September 8, 2025

Please see RM0433: bus matrix Figure 1 (pg. 105) and 22.5.  Your external SDRAM likely is connected thru the FMC.

Look for information about DMA controllers that can connect FMC and other memories.