Skip to main content
October 11, 2025
Question

Driving a Sigma-Delta ADC with STM32H562RIT6

  • October 11, 2025
  • 1 reply
  • 175 views

Hi

Please provide a sample code to interface a Sigma-Delta type ADC like the ADuM7701 with the STM32H562RIT6, which does not have a DFSDM unit, and guide me on optimizing the code so that the microcontroller is not solely occupied with processing the MDAT signal from the ADuM7701.

 
thank you

1 reply

AScha.3
Super User
October 11, 2025

Hi,

so on cpu without DFSDM  , could try using the SAI : PDM mode

AScha3_0-1760187066076.png

But:

AScha3_1-1760187099954.png

So look on git, sure you can find some pdm->decimation filter , then write your program.

+

>provide a sample code to interface a Sigma-Delta type ADC 

>and guide me on optimizing the code 

...-->

Here you can find helping hands for your project:

 

"If you feel a post has answered your question, please click ""Accept as Solution""."