Skip to main content
Explorer II
June 26, 2025
Solved

Ethernet Modes Supported for STM32H757XI

  • June 26, 2025
  • 1 reply
  • 280 views

As given on datasheet this microcontroller can support 10/100 Base T Ethernet. Is there any probability that this microcontroller supports Gigabit Ethernet and if yes, please provide the recommended circuitry for the same.

Best answer by LCE

Not possible.

H7 ETH MAC supports 100M max.

Check the STM32MPx series, (some of) these have Gigabit MACs.

Edit: maybe there's a solution with an extra IC, something like "SPI-to-Gigabit".

1 reply

LCE
LCEBest answer
Principal II
June 26, 2025

Not possible.

H7 ETH MAC supports 100M max.

Check the STM32MPx series, (some of) these have Gigabit MACs.

Edit: maybe there's a solution with an extra IC, something like "SPI-to-Gigabit".