Skip to main content
Associate III
August 4, 2025
Question

F767: Firmware Upgrade using USB-host

  • August 4, 2025
  • 3 replies
  • 387 views

Hello.. I'm designing a project using STM32F767 that upgrades firmware using USB Host 2.0. Could anyone advise on the following:

1. any application notes regarding the hardware pin connection, schematic diagram or any EVK board?

2. should i use USB_OTG_HS_DP, USB_OTG_HS_DM, USB_OTG_HS_VBus?

3. Should i use the 4 wire USB female connector? with these pins VCC, D+, D- , Gnd? Please advise soon, thx 

woldes

3 replies

Andrew Neil
Super User
August 4, 2025

Firmware Update using USB Pen drive

 

As far as the USB Host goes, the fact that you're doing firmware update would be irrelevant - you're just pulling data from the inserted device.

On the Product Page for your chosen STM32F767, go to the 'Tools & Software' tab to find recommended dev boards.

AN4879: Introduction to USB hardware and PCB guidelines using STM32 MCUs

AN4661: Getting started with STM32F7 Series MCU hardware development 

 

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate III
August 4, 2025
Andrew Neil
Super User
August 4, 2025

That's DFU - which is device-side.

 

Or are you saying that you want your STM32F767 to be able to update a device that's plugged into it?

ie, update from the STM32F767 Host to a device plugged into it?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate III
August 4, 2025

Can anyone kindly advise? 

Technical Moderator
August 5, 2025

Hi @HMSEdinburge 

This is an example firmware of DFU application on F746. It should be the same implementation as Nucleo F767.

Maybe this application note could be helpful as well.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.Best regards,FBL