Skip to main content
Associate
August 20, 2025
Question

FDCAN not working on STM32H503CBT6

  • August 20, 2025
  • 4 replies
  • 496 views

Hi, 

I'm trying to communicate two microcontrollers (STM32H503CBT6 and a NUCLEO-H503RB) via FDCAN but the STM32H503CBT6 is not sending any messages.

Both have the same configuration, but the NUCLEO-H503RB can send (I have checked it with an oscilloscope).

Searching for an answer I found this question on the forum, saying that the STM32U5F7 has the FDCAN disabled by hardware and I wonder if this is the case with the STM32H503CBT6 

Question: https://community.st.com/t5/stm32-mcus-products/fdcan-not-working-with-stm32u5f7/td-p/720224

Thanks!

4 replies

Karl Yamashita
Principal
August 20, 2025

We know that a NUCLEO-H503RB is a development board but what is a STM32H503CBT6?

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
AUJVVAuthor
Associate
August 26, 2025

 

It is the 48 pin microcontroller from STM32H5 series. 

Karl Yamashita
Principal
August 26, 2025

@AUJVV wrote:

 

It is the 48 pin microcontroller from STM32H5 series. 


So it's just the microcontroller by itself and not soldered onto a custom board? 

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
Ozone
Principal
August 26, 2025

> I'm trying to communicate two microcontrollers (STM32H503CBT6 and a NUCLEO-H503RB) via FDCAN but the STM32H503CBT6 is not sending any messages.

> Both have the same configuration, but the NUCLEO-H503RB can send (I have checked it with an oscilloscope).

Have you checked the CAN Rx input at what you call "STM32H503CBT6" with a scope while the other side sends ?
And if so, what do the REC and TEC registers in the "STM32H503CBT6" CAN peripheral say ?

MHoll.2
Senior III
August 27, 2025

the STM32H503CBT6 has a working FDCAN controller.

To help You I need more information:

1) The Nucleo-H503RB don't has a CAN Transceiver, can You show how You connected the CANBus?

2) How is the CANBus connected on You custom board (base on the STM32H503CBT6)?

 

AUJVVAuthor
Associate
August 27, 2025

I'm using the 2 transceivers TCAN1463-Q1 of Texas Instruments, one for the nucleo board and another for the custom board, same connection.

I was able to transmit with the custom board, but the signal looks like this:

tx_signal.PNG

I searched and I found out that this is probably due to the TX line, but I don't know what is causing it.

Have you ever encountered behaviour like this?

I'm clousing the post because i think that the problem is in my board.

mƎALLEm
Technical Moderator
August 27, 2025

Check your HW especially the transceiver part:

Power supply (VCC), VIO pin level voltage, EN pin, Standby pin level voltage etc..:

mALLEm_0-1756281579274.png

 

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."