Skip to main content
HYosh.2
Associate II
August 4, 2025
Solved

G071_SPI2-MOSI is not output on PA4.

  • August 4, 2025
  • 3 replies
  • 408 views

I’m working on a program to transmit data over SPI1 and SPI2 using DMA. For output I only use each peripheral’s CLK and MOSI lines. SPI1 and SPI2 differ only in the exact data being sent—their configurations and the number of bytes are identical.

Also, when driving the lines I first need to bit-bang them, so I disable the peripheral, toggle the pins by software, and then re-enable the peripheral.

With an oscilloscope I confirmed that SPI1’s CLK and MOSI, and SPI2’s CLK, all switch as expected—but SPI2’s MOSI never toggles correctly.

I believe the peripheral setup is correct, yet when I remap SPI2-MOSI from PA4 to PA10, it works perfectly.

Do you know why PA4 fails to output MOSI?

Below, (1) is the code that was active when SPI2-MOSI was on PA4 (no output), and (2) is the code active when on PA10 (correct output).

The PCB layout is already fixed, so if PA4 can’t serve as SPI2-MOSI it’s a serious problem.

Now, I'm using Nucleo-G071RB for test.

Any insights would be greatly appreciated.

InitialConfig bellow code

 
 /****************************/
 /** SPI1 GPIO Configuration */
 /****************************/
 /* PA5 ------> SPI1_SCK */
 /* PA7 ------> SPI1_MOSI */

 LL_SPI_InitTypeDef SPI1_InitStruct = {0};
 LL_GPIO_InitTypeDef GPIO_InitStruct_SPI1 = {0};

 /* Peripheral clock enable */
 LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_SPI1);

 GPIO_InitStruct_SPI1.Pin = LL_GPIO_PIN_5;
 GPIO_InitStruct_SPI1.Mode = LL_GPIO_MODE_ALTERNATE;
 GPIO_InitStruct_SPI1.Speed = LL_GPIO_SPEED_FREQ_HIGH;
 GPIO_InitStruct_SPI1.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
 GPIO_InitStruct_SPI1.Pull = LL_GPIO_PULL_NO;
 GPIO_InitStruct_SPI1.Alternate = LL_GPIO_AF_0;
 LL_GPIO_Init(GPIOA, &GPIO_InitStruct_SPI1);

 GPIO_InitStruct_SPI1.Pin = LL_GPIO_PIN_7;
 GPIO_InitStruct_SPI1.Mode = LL_GPIO_MODE_ALTERNATE;
 GPIO_InitStruct_SPI1.Speed = LL_GPIO_SPEED_FREQ_HIGH;
 GPIO_InitStruct_SPI1.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
 GPIO_InitStruct_SPI1.Pull = LL_GPIO_PULL_NO;
 GPIO_InitStruct_SPI1.Alternate = LL_GPIO_AF_0;
 LL_GPIO_Init(GPIOA, &GPIO_InitStruct_SPI1);

 /* SPI1 DMA Init */
 LL_DMA_SetPeriphRequest(DMA1, LL_DMA_CHANNEL_1, LL_DMAMUX_REQ_SPI1_TX);
 LL_DMA_SetPeriphAddress(DMA1, LL_DMA_CHANNEL_1, (uint32_t)&SPI1->DR);
 LL_DMA_SetDataTransferDirection(DMA1, LL_DMA_CHANNEL_1, LL_DMA_DIRECTION_MEMORY_TO_PERIPH);
 LL_DMA_SetChannelPriorityLevel(DMA1, LL_DMA_CHANNEL_1, LL_DMA_PRIORITY_MEDIUM);
 LL_DMA_SetMode(DMA1, LL_DMA_CHANNEL_1, LL_DMA_MODE_NORMAL);
 LL_DMA_SetPeriphIncMode(DMA1, LL_DMA_CHANNEL_1, LL_DMA_PERIPH_NOINCREMENT);
 LL_DMA_SetMemoryIncMode(DMA1, LL_DMA_CHANNEL_1, LL_DMA_MEMORY_INCREMENT);
 LL_DMA_SetPeriphSize(DMA1, LL_DMA_CHANNEL_1, LL_DMA_PDATAALIGN_BYTE);
 LL_DMA_SetMemorySize(DMA1, LL_DMA_CHANNEL_1, LL_DMA_MDATAALIGN_BYTE);

 /* SPI1 parameter configuration*/
 SPI1_InitStruct.TransferDirection = LL_SPI_FULL_DUPLEX;
 SPI1_InitStruct.Mode = LL_SPI_MODE_MASTER;
 SPI1_InitStruct.DataWidth = LL_SPI_DATAWIDTH_8BIT;
 SPI1_InitStruct.ClockPolarity = LL_SPI_POLARITY_LOW;
 SPI1_InitStruct.ClockPhase = LL_SPI_PHASE_2EDGE;
 SPI1_InitStruct.NSS = LL_SPI_NSS_SOFT;
 SPI1_InitStruct.BaudRate = LL_SPI_BAUDRATEPRESCALER_DIV8; /* SYSCLK32MHz ÷ 8 = 4MHz*/
 SPI1_InitStruct.BitOrder = LL_SPI_MSB_FIRST;
 SPI1_InitStruct.CRCCalculation = LL_SPI_CRCCALCULATION_DISABLE;
 SPI1_InitStruct.CRCPoly = 7;
 LL_SPI_Init(SPI1, &SPI1_InitStruct);
 LL_SPI_SetStandard(SPI1, LL_SPI_PROTOCOL_MOTOROLA);
 LL_SPI_DisableNSSPulseMgt(SPI1);

 LL_SPI_Enable(SPI1); 
 LL_SPI_EnableDMAReq_TX(SPI1);

 /*****************************/
 /** SPI2 GPIO Configuration **/
 /*****************************/
 /* PA0 ------> SPI2_SCK */
 /* PA4 ------> SPI2_MOSI */

 LL_SPI_InitTypeDef SPI2_InitStruct = {0};
 LL_GPIO_InitTypeDef GPIO_InitStruct_SPI2 = {0};

 /* Peripheral clock enable */
 LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_SPI2);

 GPIO_InitStruct_SPI2.Pin = LL_GPIO_PIN_0;
 GPIO_InitStruct_SPI2.Mode = LL_GPIO_MODE_ALTERNATE;
 GPIO_InitStruct_SPI2.Speed = LL_GPIO_SPEED_FREQ_HIGH;
 GPIO_InitStruct_SPI2.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
 GPIO_InitStruct_SPI2.Pull = LL_GPIO_PULL_NO;
 GPIO_InitStruct_SPI2.Alternate = LL_GPIO_AF_0;
 LL_GPIO_Init(GPIOA, &GPIO_InitStruct_SPI2);

 GPIO_InitStruct_SPI2.Pin = LL_GPIO_PIN_4; //(1)when using PA4 as SPI2_MOSI
 // GPIO_InitStruct_SPI2.Pin = LL_GPIO_PIN_10; //(2)when using PA10 as SPI2_MOSI
 GPIO_InitStruct_SPI2.Mode = LL_GPIO_MODE_ALTERNATE;
 GPIO_InitStruct_SPI2.Speed = LL_GPIO_SPEED_FREQ_HIGH;
 GPIO_InitStruct_SPI2.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
 GPIO_InitStruct_SPI2.Pull = LL_GPIO_PULL_NO;
 GPIO_InitStruct_SPI2.Alternate = LL_GPIO_AF_1; //(1)when using PA4 as SPI2_MOSI
 // GPIO_InitStruct_SPI2.Alternate = LL_GPIO_AF_0; //(2)when using PA10 as SPI2_MOSI
 LL_GPIO_Init(GPIOA, &GPIO_InitStruct_SPI2);

 /* SPI2 DMA Init */
 LL_DMA_SetPeriphRequest(DMA1, LL_DMA_CHANNEL_2, LL_DMAMUX_REQ_SPI2_TX);
 LL_DMA_SetPeriphAddress(DMA1, LL_DMA_CHANNEL_2, (uint32_t)&SPI2->DR);
 LL_DMA_SetDataTransferDirection(DMA1, LL_DMA_CHANNEL_2, LL_DMA_DIRECTION_MEMORY_TO_PERIPH);
 LL_DMA_SetChannelPriorityLevel(DMA1, LL_DMA_CHANNEL_2, LL_DMA_PRIORITY_MEDIUM);
 LL_DMA_SetMode(DMA1, LL_DMA_CHANNEL_2, LL_DMA_MODE_NORMAL);
 LL_DMA_SetPeriphIncMode(DMA1, LL_DMA_CHANNEL_2, LL_DMA_PERIPH_NOINCREMENT);
 LL_DMA_SetMemoryIncMode(DMA1, LL_DMA_CHANNEL_2, LL_DMA_MEMORY_INCREMENT);
 LL_DMA_SetPeriphSize(DMA1, LL_DMA_CHANNEL_2, LL_DMA_PDATAALIGN_BYTE);
 LL_DMA_SetMemorySize(DMA1, LL_DMA_CHANNEL_2, LL_DMA_MDATAALIGN_BYTE);

 /* SPI2 parameter configuration*/
 SPI2_InitStruct.TransferDirection = LL_SPI_FULL_DUPLEX;
 SPI2_InitStruct.Mode = LL_SPI_MODE_MASTER;
 SPI2_InitStruct.DataWidth = LL_SPI_DATAWIDTH_8BIT;
 SPI2_InitStruct.ClockPolarity = LL_SPI_POLARITY_LOW;
 SPI2_InitStruct.ClockPhase = LL_SPI_PHASE_2EDGE;
 SPI2_InitStruct.NSS = LL_SPI_NSS_SOFT;
 SPI2_InitStruct.BaudRate = LL_SPI_BAUDRATEPRESCALER_DIV8; /* SYSCLK32MHz ÷ 8 = 4MHz*/
 SPI2_InitStruct.BitOrder = LL_SPI_MSB_FIRST;
 SPI2_InitStruct.CRCCalculation = LL_SPI_CRCCALCULATION_DISABLE;
 SPI2_InitStruct.CRCPoly = 7;
 LL_SPI_Init(SPI2, &SPI2_InitStruct);
 LL_SPI_SetStandard(SPI2, LL_SPI_PROTOCOL_MOTOROLA);
 LL_SPI_DisableNSSPulseMgt(SPI2);

 LL_SPI_Enable(SPI2); 
 LL_SPI_EnableDMAReq_TX(SPI2);

below code are function of changing to bitbangmode.

/**************************************************/

void SpiEnterBitBang(void) {
 /* SPI停止 */
 LL_SPI_Disable(SPI1);
 LL_SPI_Disable(SPI2);

 /* GPIOモードへ設定: */
 LL_GPIO_SetPinMode(GPIOA, LL_GPIO_PIN_5, LL_GPIO_MODE_OUTPUT);
 LL_GPIO_SetPinMode(GPIOA, LL_GPIO_PIN_7, LL_GPIO_MODE_OUTPUT);
 LL_GPIO_SetPinMode(GPIOA, LL_GPIO_PIN_0, LL_GPIO_MODE_OUTPUT);
 LL_GPIO_SetPinMode(GPIOA, LL_GPIO_PIN_4, LL_GPIO_MODE_OUTPUT); //(1)when using PA4 as SPI2_MOSI
 // LL_GPIO_SetPinMode(GPIOA, LL_GPIO_PIN_10, LL_GPIO_MODE_OUTPUT); //(2)when using PA10 as SPI2_MOSI
};

void SpiExitBitBang(void) {
 /* SPI出力モードへ再設定 */
 LL_GPIO_SetPinMode(GPIOA, LL_GPIO_PIN_5, LL_GPIO_MODE_ALTERNATE);
 LL_GPIO_SetAFPin_0_7(GPIOA, LL_GPIO_PIN_5, LL_GPIO_AF_0);

 LL_GPIO_SetPinMode(GPIOA, LL_GPIO_PIN_7, LL_GPIO_MODE_ALTERNATE);
 LL_GPIO_SetAFPin_0_7(GPIOA, LL_GPIO_PIN_7, LL_GPIO_AF_0);

 LL_GPIO_SetPinMode(GPIOA, LL_GPIO_PIN_0, LL_GPIO_MODE_ALTERNATE);
 LL_GPIO_SetAFPin_0_7(GPIOA, LL_GPIO_PIN_0, LL_GPIO_AF_0);

 LL_GPIO_SetAFPin_0_7(GPIOA, LL_GPIO_PIN_4, LL_GPIO_AF_1); //(1)when using PA4 as SPI2_MOSI
 LL_GPIO_SetPinMode(GPIOA, LL_GPIO_PIN_4, LL_GPIO_MODE_ALTERNATE); //(1)when using PA4 as SPI2_MOSI
 // LL_GPIO_SetPinMode(GPIOA, LL_GPIO_PIN_10, LL_GPIO_MODE_ALTERNATE); // (2)when using PA10 as SPI2_MOSI
 // LL_GPIO_SetAFPin_0_7(GPIOA, LL_GPIO_PIN_10, LL_GPIO_AF_0); //(2)when using PA10 as SPI2_MOSI

 /* SPI有効化 */
 LL_SPI_Enable(SPI1);
 LL_SPI_Enable(SPI2);
};

This post has been edited to add the right labels and apply source code formatting, please see How to insert source code.

Best answer by HYosh.2

I overlooked the note in the attached section. I’ll look into disabling the DAC during SPI transmissions. Thank you for your support.

HYosh2_0-1754408875515.png

 

3 replies

waclawek.jan
Super User
August 4, 2025

What hardware is this, your own, or some "known good" board such as Nucleo or Disco?

Does PA4 work "normally" when you set it as GPIO Output and toggle "manually"?

Read out and check/post content of SPI and relevant GPIO registers.

JW

HYosh.2
HYosh.2Author
Associate II
August 4, 2025

I’m currently testing on a Nucleo-G071RB and will eventually port everything to a custom board based on the STM32G071GBU3. As you suggested, I tried to bit-bang PA4—but while I could control other pins, PA4 wouldn’t toggle. Could this be related to the DAC?

I’m using DAC channel 1 as the COMP negative input.

/*****************************/
/** DAC channel OUT1 config **/
/*****************************/
LL_DAC_InitTypeDef DAC_InitStruct = {0};
LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_DAC1); /* Peripheral clock enable */

DAC_InitStruct.TriggerSource = LL_DAC_TRIG_SOFTWARE;
DAC_InitStruct.WaveAutoGeneration = LL_DAC_WAVE_AUTO_GENERATION_NONE;
DAC_InitStruct.OutputBuffer = LL_DAC_OUTPUT_BUFFER_DISABLE;
DAC_InitStruct.OutputConnection = LL_DAC_OUTPUT_CONNECT_INTERNAL;
DAC_InitStruct.OutputMode = LL_DAC_OUTPUT_MODE_NORMAL;
LL_DAC_Init(DAC1, LL_DAC_CHANNEL_1, &DAC_InitStruct);
LL_DAC_DisableTrigger(DAC1, LL_DAC_CHANNEL_1);

LL_DAC_Enable(DAC1, LL_DAC_CHANNEL_1); /* DAC動作開始 */
LL_DAC_ConvertData12RightAligned(DAC1, LL_DAC_CHANNEL_1, 0x800); /* VDD x 0.5Vに設定 */
LL_DAC_TrigSWConversion(DAC1, LL_DAC_CHANNEL_1); /* 変換実行 */



waclawek.jan
Super User
August 4, 2025

> Could this be related to the DAC?

Indeed, that will be it, as a consequence of the GPIO assigned to DAC cannot be used in output mode when the DAC output is connected to on-chip peripheral erratum.

 

JW

HYosh.2
HYosh.2Author
Associate II
August 5, 2025

I rechecked the reference manual, and it states that setting the DAC_MCR MODE register to 0b011 disables the buffer and routes the DAC only to on-chip peripherals. I confirmed in the debugger that DAC1_CH1.MODE is indeed set to 0b011, so is it still impossible to use PA4 with other peripherals under these conditions?

 

DAC_MODE.png

waclawek.jan
Super User
August 5, 2025

Errata explain deviations from the reference manual (which describes the design intention), thus errata "override" the manual.

Have you read the quoted erratum?

JW

HYosh.2
HYosh.2AuthorBest answer
Associate II
August 5, 2025

I overlooked the note in the attached section. I’ll look into disabling the DAC during SPI transmissions. Thank you for your support.

HYosh2_0-1754408875515.png