HAL_Flash_Program triggers HardFault exception
- June 11, 2024
- 3 replies
- 4165 views
Hello everyone,
I'm facing a weird issue about Flash programming on a STM32g0b1 microcontroller on IAR Workbench for ARM.
Context
I'm working on a bootloader project. I am able to lock, unlock, erase and program flash at the beginning of my program. Following a state machine, this is working well.
Issue
When it comes to save a new bunch of data for the second time (I always program by block of 256 bytes so 32 double-words which is required by the library), it triggers a HardFault exception
Remark 1
If I go step by step in debug mode, I can program double-word by double-word without any exception. But if I run the program without going step by step (going over the function or without triggering any breakpoint), I automatically trigger the exception. And when the exception is triggered, no double-word has been written to flash so it is cancelled from the beginning
Remark 2
What is weird is that I'm able to fully erase flash (without touching the program of course) and to program few datas at different location without any issue. It only comes to it when reaching this special part of my program. And as I said, in any case, I'm writing 256 bytes (divided in 32 double-words)
Remark 3
I checked FLASH_SR and FLASH_CR register, it seems to not detect any issue. Also, interrupts are correctly disable before performing a program. I also increase Heap/stack size and nothing changed.
I'm starting to run out of idea. Can you help me to find a solution please?
Thanks in advance and have a good day !
Adrien