Skip to main content
Associate II
August 5, 2025
Question

How does stm32H723 ADC ISR know which channel ?

  • August 5, 2025
  • 3 replies
  • 460 views

I am just getting started with the stm32h723 ADC.    If I create a regular sequence group of several input channels, how does my ISR know which channel was sampled last (which channel's data is in the DR)?  I don't see this in the registers.

Thanks,

Mark 

3 replies

Tesla DeLorean
Guru
August 5, 2025

Typically you'd DMA a group of channels into an array, and then get an interrupt for some multiple of them.

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
NiramasAuthor
Associate II
August 5, 2025

So I have to go down another rabbit hole to get my ADC data?   Is there a code example for the ADC-DMA transfer?

Tesla DeLorean
Guru
August 5, 2025

Not sure it's a rabbit hole, just not an 8-bit programming / 1-dimensional approach.

The concept is to allow for decimation of interrupt loading, and allow for more rapid/consistent cycling of the ADC, ie uniform sample rate so time-domain based analysis is workable.

Now if you want to sample individual channels on ADC1, ADC2, ADCn, then you can do that.

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
Technical Moderator
August 5, 2025

Hello @Niramas ,

You can get inspired from the "ADC DMA Transfer" example runs on STM32H743xx devices:

STM32CubeH7/Projects/NUCLEO-H743ZI/Examples/ADC/ADC_DMA_Transfer at master · STMicroelectronics/STM32CubeH7 · GitHub

This example can be easily tailored to any other supported device and development board.

"When your question is answered, please close this topic by clicking ""Accept as Solution"".ThanksImen"
NiramasAuthor
Associate II
August 5, 2025

So are the examples for any STM32H7 variant applicable to the STM32H723?    I was only looking in the 723 examples folder.

Technical Moderator
August 5, 2025

You can use the ADC example from STM32H735 device which is a pin-to-pin compatible with STM32H723:

STM32CubeH7/Projects/STM32H735G-DK/Examples/ADC/ADC_DMA_Transfer at master · STMicroelectronics/STM32CubeH7 · GitHub

But always consult the datasheets and reference manuals for detailed comparison.

"When your question is answered, please close this topic by clicking ""Accept as Solution"".ThanksImen"