Skip to main content
Associate II
July 3, 2025
Solved

How to achieve repeated START after IBI with STM32H503 I3C controller

  • July 3, 2025
  • 2 replies
  • 461 views

Hello everyone, I'm using two STM32H503 boards.  One is programmed as an I3C controller, the other as an I3C target, and I'm trying to achieve the following sequence on the I3C bus: IBI from target -> Repeated Start -> Private Read 

Harry0709_3-1751533080897.png

 

I find two things in RM0492 that may be helpful for my question: One is in Figure 418, there is the following note with 2 asterisks :Repeated start (Sr) if there is a pending transfer to execute and if I3C_DEVRi.SUSP = 0, else stop (P) in push-pull.

Harry0709_1-1751532228758.png

The other is that there is a register called I3C device x characteristics register in RM0492. Here is the following description in RM0492, I set bit19 SUSP to 0, so that C-FIFO and TX-FIFO are not flushed after an IBI request.

Harry0709_2-1751532265177.png

Based on this description, I preload a private read with C-FIFO before IBI, but I still saw that IBI completes with STOP, and then a START with private read. Is it possible to generate a repeated start after an IBI request? Does Hardware support for this sequence?

 

 

 

Best answer by KDJEM.1

Hello @Harry0709 and welcome to the community,

 

First of all, I apologize for my late reply.

The pending read IBI always ends with STOP. The software then needs to program a read to the target that requested the pending read. No possibility to have a RESTART between the IBI and the private read.

I hope this answer your request!

 

Thank you.

Kaouthar

2 replies

KDJEM.1
KDJEM.1Best answer
Technical Moderator
August 29, 2025

Hello @Harry0709 and welcome to the community,

 

First of all, I apologize for my late reply.

The pending read IBI always ends with STOP. The software then needs to program a read to the target that requested the pending read. No possibility to have a RESTART between the IBI and the private read.

I hope this answer your request!

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
KDJEM.1
Technical Moderator
September 26, 2025

Hello @Harry0709 ;

 

Is my reply answered your request? 

If yes, please click on Accept as Solution on the reply which answered your question.

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.