Skip to main content
Associate III
September 24, 2025
Question

How to use external reference voltage for ADC (Nucleo-H723ZG)

  • September 24, 2025
  • 1 reply
  • 252 views

I want to provide external reference voltage to 16-bit ADC.

sreyas40_0-1758697683463.png

So i need to remove the  R36.

sreyas40_1-1758697754486.png

And Vref is connected to Vref+ pin on the board.

These two things are the only steps i need to do right, after that i have to connect my external source to the vref+ pin and it will be the reference voltage for my ADC. 

sreyas40_3-1758698218843.png

And i need to make sure Vref<= Vdda, small increase might not be an issue right?  Are there anything else i need to look into

1 reply

LCE
Principal II
September 24, 2025

Looks okay at first glance.

small increase might not be an issue right

Read the datasheet...

The problem with this on a Nucleo board might be, that (probably, not sure) the external VREF's capacitor is far away from the VREF pin.

The supply voltage isn't too bad / noisy, so depending on the routing of the VREF at the connector and where its cap is placed, it might make things worse.