If pullup is enabled on gpio for SPI Clock, does pullup have any effect while spi is enabled?
Say I am operating as master with CPOL=1. Because the NSS pin seems to lag the enable bit (SPE) slightly, my logic analyzer always barfs on the first SPI packet because the clock is in the wrong state.
So, I set the GPIO to have a pullup on the clock in CubeMX and the problem goes away - as soon as the init functions run, the clock goes high and stays that way until the first SPI transmit. Also, the clock stays high after the end of the transfer if the SPI is disabled in the callback function.
My only concern is for power consumption: It is obvious that the pullup gets applied when the SPI is disabled but I don't know is if the pullup applied all the time even when the alternate mode of the GPIO is set, i.e. is the pullup still applied at the pin when the SPI is enabled? Do clock pulses during an SPI transaction work against the pullup?