Skip to main content
HungKai.Chien
Associate II
July 31, 2025
Solved

Inquiry on STM32G0 Support for Dual USB-C Ports with DRP and DP-Alt Mode

  • July 31, 2025
  • 3 replies
  • 335 views

I am currently evaluating the STM32G0 series for a project that requires two USB Type-C ports.
Each port needs to support both Dual Role Port (DRP) functionality and DisplayPort Alternate Mode (DP-Alt).
Can the STM32G0 be implemented?

Best answer by FBL

Hi @HungKai.Chien 

Indeed, it is the same controller available on both ports. So, they have the same features.

3 replies

Technical Moderator
August 1, 2025

Hi @HungKai.Chien 

Indeed, STM32G0 is the only product using 2 USB type C ports.

You can refer to the MB1352 schematics of STM32G0C1 eval daughter board as a reference.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.Best regards,FBL
HungKai.Chien
Associate II
August 4, 2025

Hi Support team,


Does each UCPD port on STM32G0C1 support both DRP and DP-Alt mode independently?”

FBLBest answer
Technical Moderator
August 4, 2025

Hi @HungKai.Chien 

Indeed, it is the same controller available on both ports. So, they have the same features.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.Best regards,FBL