Is that possible to inject five volt level of external clock on OSC_IN?
Hi,
I need to use a 5V external clock for an stm32g473. The datasheet in table 39. High-speed external user clock characteristics says Vhsel is max Vdd, but Table 12. STM32G473xB/xC/xE pin definition says PF0 / OSC_IN is FT_a (five volt tolerant).
Is it safe to use an external 5V clock ?
Thx,