Skip to main content
Associate
August 2, 2025
Question

LCD-TFT project with 1024x768 resolution. Which MCU to use?

  • August 2, 2025
  • 3 replies
  • 466 views

Hi guys, sorry if I'm posting this in the wrong area.

I'm starting a project that uses a 1024x768 graphics display and I was wondering which STM32F MCU  (LQFP 176pin) would be the better to drive the RGB Panel. I would be using external memory but if there is a MCU with internal memory that can display 1024x768 that would be easier and would make the project cheaper as well.

Can you please let me know as soon as possible as at this stage I'm doing the research on what I need before I purchase all the parts.

Thanks guys and hope to hear from you soon.

Peter

 

3 replies

AScha.3
Super User
August 3, 2025

Hi,

so for a 1024x768 pix display, the first question is : what it should show ?

Maybe hi-speed video or animation for a game - or GUI for process or machine controlling ?

So for a GUI , and using a "small " cpu (compared to the SOCs used in mobile phones) , its good idea, to use a display with onboard graphics and frame buffer , so the cpu just giving graphic commands to the display, connected with a SPI .

I use the TFTs with EVE graphics, the TFT has almost same price range as a plain "***" TFT frame.

Just look at mouser...

btw 1024x768 seems very unusual , more is : 800x480 , 1024x600 or 1280x800 ;

AScha3_0-1754205647681.png

https://www.mouser.de/c/optoelectronics/displays/lcd-displays/?diagonal=7%20in%7C~10.1%20in&m=Newhaven%20Display%7C~Riverdi&instock=y&sort=pricing&pg=2

 

or look at displays, with STM cpu already there...

AScha3_1-1754205942118.png

https://riverdi.com/de/produkt-kategorie/stm32-embedded-displays-de?sort_order=_sfm__regular_price+asc+num

 

... many others also, just ask google :)

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
AcelinkAuthor
Associate
August 4, 2025

Thanks for the info but it's not what I'm looking for. They have 8080 or 6800 16bit interfaces which is just to slow for our project. 

Thanks for the info anyway.

Peter :)

 

MM..1
Chief III
August 3, 2025

You ask MCU then STM32U5 is only one with internal RAM sized for single buffer RGB565 optimaly, or moremore power new N6...

Display you can choice RGB or better DSI.

AcelinkAuthor
Associate
August 4, 2025

Thanks for the info. I just checked out a few of the STM32U5 and none that I reviewed uses the RGB interface, only MIPI. Our project uses RGB interface with Hsync, Vsync signals.

Also the STM32N6 series is BGA package so we can't prototype with it. Only LQFP 144pin or 176pin.

Do you have any other suggestions? 

Peter :)

 

AScha.3
Super User
August 4, 2025

So look yourself...

https://www.st.com/content/st_com/en/stm32-mcu-product-selector.html

with RGB par. -> maybe STM32H7R3Z8 , 144pin lqfp.

 

AScha3_0-1754300644711.png

 

"If you feel a post has answered your question, please click ""Accept as Solution""."