Skip to main content
Visitor II
July 19, 2025
Question

Nucleo LD1 Light dims after sometime and St-link is not recognized by the laptop

  • July 19, 2025
  • 1 reply
  • 200 views

I have an STM32F401 nucleo board and it used to work fine but now after a minute of connecting it with usb, the LD1 suddenly dims to very low light like pin on float. Before that it works fine, I can program it, debug it.

1 reply

Amel NASRI
Technical Moderator
July 23, 2025

Hi @Lakshay ,

Try using STM32CubeProgrammer to check if you can connect to the board. Probably you need ST-Link firmware upgrade.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.