Question
Question on 4.7uF ceramic capacitor
- April 3, 2026
- 1 reply
- 435 views
Post edited by ST moderator: title and post edited to translate the content.
我在stm32F412RGT6的数据手册的6.1.6部分看到关于滤波电容的描述,2. The 4.7 µF ceramic capacitor must be connected to one of the VDD pin.从图中来看是以144PIN的芯片为例,但我使用的是64PIN的封装,是否也需要在其中一个VDD引脚放置4.7uf的电容,如果需要,是单独放置一个4.7uf还是与一个0.1uf并联放置
Translation:
"In section 6.1.6 of the STM32F412RGT6 datasheet, regarding filter capacitors, it states: "2. The 4.7 µF ceramic capacitor must be connected to one of the VDD pins." The diagram shows this for a 144-pin chip, but I'm using a 64-pin package. Do I also need to place a 4.7 µF capacitor on one of the VDD pins? If so, should I place a single 4.7 µF capacitor or connect it in parallel with a 0.1 µF capacitor?"