Reading clock input on OSC_IN
Hi,
I have an stm32g473 which use the clock of another system as external clock on PF0 / OSC_IN. This clock is them multiplied by 74 through the PLL. I need to synchronize my code with the external clock (i.e. wait for it to rise).
What is the simplest way to do this? Can I use PF0 both as OSC_IN and as an GPIO in input mode to generate an event on the rising edge? or should I root the clock to both OSC_IN and another GPIO?
Are there other possibilities did not find in the reference manual (e.g. using the HSE as a trigger to one of the timer or an event I could WFE on ?)
Thanks.