Skip to main content
Associate III
July 31, 2025
Question

Resistor configurarion used for VBUS configuracion

  • July 31, 2025
  • 2 replies
  • 344 views

Hi, I´m reading the following document : "an4879-introduction-to-usb-hardware-and-pcb-guidelines-using-stm32-mcus-stmicroelectronics" to implement USB in my application. 

In section 2.6.1 Simple Resistor Divider it says "This solution works well as long as GPIO maximum operating conditions are >= VDD+ 3.6 V" this must be meet to use the following voltage dividider 

Aldo_Flores_Aguayo_0-1753998318971.png

I´m going to use PA9 pin, in the datasheet of my MCU STM32L4P5RGT6 it states this pin is 5V tolerant 

As I understood this pin doesnt meet the condiciton mentioned before because my VDD=3.3V and so GPIO maximum operating condition should be >= VDD+3.6V so we have 3.3+3.6V=6.9V so 5V < 6.9V so I can't use this configuration do I understand this well ? 

 

Should I use this other configuration? 

Aldo_Flores_Aguayo_1-1753998839473.png

I´m a bit confused about it hope some one could help me to clarify this. 

 

2 replies

TDK
Super User
July 31, 2025

It'll work.

 

PA9 is a 5V tolerant pin.

TDK_0-1754001545310.png

So incoming voltage limits are VDD + 4.0 V:

TDK_1-1754001576612.png

 

Voltage there will never be more than 3.75 V, as long as VBUS respects USB limits (4.75 V to 5.25 V).

 

The issue here is ensuring the voltage on the pin is acceptable when the device is off. This is satisfied.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Technical Moderator
August 1, 2025

HI @Aldo_Flores_Aguayo 

PA9 is a five volt-tolerant pin, including an additional function natively dedicated to VBUS sensing.

The absolute maximum ratings table of the datasheet indicates that the five volt-tolerant pin voltage cannot exceed VDD+ 4V.

You can check the schematics of STM32L4P5 Disco board provided as reference:

FBL_0-1754042902139.png

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.Best regards,FBL
Associate III
August 9, 2025

Thanks for your replies @FBL @TDK 

Okay, I think I got it, so just one question why in one parte of the"  introduction to USB hardware" it shows the following

Aldo_Flores_Aguayo_0-1754773209881.png

 

"five volt-tolerant pin voltage cannot exceed
VDD + 4 V."

 

And then in the MCU datasheet the the following appears with respect to five volt tolerant pins 

Aldo_Flores_Aguayo_1-1754773281870.png

 

So it´s VDD+4V or min(VDD) +4V ??

 

Hope you can clarify this, thanks for your time.

 

TDK
Super User
August 9, 2025

> There is a notable difference when using VDD+4V or min(VDD)+4V.

Think they're the same. When the chip is not powered, VDD = 0. The datasheet has the details.

"If you feel a post has answered your question, please click ""Accept as Solution""."