Skip to main content
Associate
August 26, 2025
Solved

SPI Always Reads 0

  • August 26, 2025
  • 1 reply
  • 306 views

I am having a problem reading SPI data on an STM32F407 where it always returns 0x00. I actually have this working using HAL on the same hardware, however for legacy reasons I need to get this working with SPL. This application is just sending clock signals to the slave and reading the received data. There is no activity on MOSI.

I can scope the signals and see the expected traffic on the SCK and MISO so I at least know my clock transmit is working. I just can grab the correct read data. Here is my code. I feel like I'm missing something basic for SPL. Any insight would be helpful.

#include "main.h"
#include "stm32f4xx_spi.h"
#include "stm32f4xx_usart.h"
#include "config.h"
#include "board_init.h"
#include "gpio.h"

#define TIMEOUT_TIME 1000;

uint16_t SPI_TransmitReceiveByte(uint16_t data);

uint16_t spiData;

void main()
{ 
 uint32_t loopCounter = 0;
 
 SystemInit();

 init_IO();
 SPI3_Init();
 powerOnLED();
 
 while (1) 
 { 
 loopCounter++;
 
 if (loopCounter == 10000)
 {
 spiData = SPI_TransmitReceiveByte(0x0000);
 loopCounter = 0;
 if (spiData != 0) powerOffLED();
 }
 }
}

uint16_t SPI_TransmitReceiveByte(uint16_t data) {
 uint32_t timeout = TIMEOUT_TIME;
 uint8_t dummy;
 
 timeout = TIMEOUT_TIME;
 while (SPI_I2S_GetFlagStatus(SPI3, SPI_I2S_FLAG_RXNE) != RESET) 
 {
 dummy = *(volatile uint8_t *)&SPI3 -> DR;
 }
 
 timeout = TIMEOUT_TIME;
 while ((SPI_I2S_GetFlagStatus(SPI3, SPI_I2S_FLAG_TXE) == RESET) & (timeout != 0)) {
 timeout--;
 }
 
 SPI_SendData(SPI3, data);
 timeout = TIMEOUT_TIME;
 
 while ((SPI_I2S_GetFlagStatus(SPI3, SPI_I2S_FLAG_RXNE) == RESET) & (timeout != 0)) {
 timeout--;
 }
 
 return SPI_ReceiveData(SPI3);
}

void SPI3_Init()
{
 GPIO_InitTypeDef spi3_io;
 SPI_InitTypeDef SPI_InitStructure;
 
 RCC_APB1PeriphClockCmd(RCC_APB1Periph_SPI3, ENABLE);
 RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE);
 
 // Configure SPI pins (SCK, MISO, MOSI)
 // Example for SPI3 on PC10, PC11, PC12
 spi3_io.GPIO_Pin = GPIO_Pin_10 | GPIO_Pin_12 | GPIO_Pin_12;
 spi3_io.GPIO_Mode = GPIO_Mode_AF;// Alternate Function
 spi3_io.GPIO_OType = GPIO_OType_PP;
 spi3_io.GPIO_PuPd = GPIO_PuPd_DOWN;
 spi3_io.GPIO_Speed = GPIO_Speed_50MHz;
 GPIO_Init(GPIOC, &spi3_io);
 
 // Connect SPI pins to alternate function
 GPIO_PinAFConfig(GPIOC, GPIO_PinSource10, GPIO_AF_SPI3);
 GPIO_PinAFConfig(GPIOC, GPIO_PinSource11, GPIO_AF_SPI3);
 GPIO_PinAFConfig(GPIOC, GPIO_PinSource12, GPIO_AF_SPI3);
 
 SPI_DeInit(SPI3); // De-initialize SPI3 first

 SPI_InitStructure.SPI_Mode = SPI_Mode_Master;
 SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex;
 SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b;
 SPI_InitStructure.SPI_CPOL = SPI_CPOL_Low; // Clock Polarity (adjust based on slave device)
 SPI_InitStructure.SPI_CPHA = SPI_CPHA_1Edge; // Clock Phase (adjust based on slave device)
 SPI_InitStructure.SPI_NSS = SPI_NSS_Soft; // Software NSS control
 SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_32; // Adjust for desired speed
 SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB;
 SPI_InitStructure.SPI_CRCPolynomial = 7; // CRC polynomial (optional)
 
 SPI_Init(SPI3, &SPI_InitStructure);
 SPI_Cmd(SPI3, ENABLE); // Enable SPI3
}
Best answer by twjudge

Please ignore. I found the error in the SPI pin setup shortly after this post. PC11 was not setup properly.

1 reply

twjudgeAuthorBest answer
Associate
August 26, 2025

Please ignore. I found the error in the SPI pin setup shortly after this post. PC11 was not setup properly.