SPI using hardware SS and GPDMA triggered by a timer
Hi all,
I am using an STM32H5 micro. I need to send out a buffer of data at regular intervals. I use TIM15 to trigger the GPDMA which sends blocks of 6 bytes to the SPI. The SPI is programmed with TSIZE=6 to get the SS output low during the transmission. I absolutely need this. The screenshot below is the result from my code.

My problem is that the SPI only works ONCE. It seems to be stuck afterwards, I observe that CSTART of the SPI goes to 0. How can I get the SPI going on with TSIZE > 0 ?