Skip to main content
Associate III
June 25, 2025
Solved

STM32 Interleaved ADC Sample Timestamping

  • June 25, 2025
  • 2 replies
  • 619 views

Hi, I am using STM32L476RG-Nucleo64 boards for one of my ultrasound projects. Basically, the process is:

1)Send 2MHz pulses with pwm

2) Sample 1000points with 8-bit interleaved ADC(500 each) and DMA

3) Send ADC data through SPI.

4) Wait TIM3 to trigger again for both ADC and PWM and back to 1

Everything is working fine, only problem is that I need the time label of each sample -Or somehow calculate the Δt between them- in ADC so that I can identify the Δt of some peaks positions in the data but it is troubling me because of maxed ADC speed

I made ADC interleaved, 8-bit and 2.5 cycles to work at max speed, not like a timer-triggered ADC. Therefore I cannot measure the total 1000 sampling time for dividing by 1000 (Not sure if all samplings are done with same speed tho).

I tried to measure the time using DMA callback and ADC callback using DWT but it is saying that the time is around 35ms and I know it is wrong because I can confirm with an oscilloscope that the data window I am sampling with 1000 sampling is around 60us.

You can review the stm32 main.c from here: main.c

Note: In the code I enabled ContiniousConvMode even though it is not recommended for triggered ADC but somehow my version works with continious mode enabled and stops working when it is disabled.

 

Also -Maybe I am misinterpreting some concepts- but my real sampling rate seems to be a lot higher than my calculations. I set 8-bit ADC interleaved with 2.5 sampling cycle and 2 cycle delay, which should give 16 cycle for 2ADC which is 10MHz sampling rate with 80MHz clock. With this setup 100 samples should take 10us, but when I compare this with an oscilloscope, 10us difference is 150 samples which is 1.5x higher than it should be.

Best answer by TDK

There are 16 cycles between the start of ADC1 sampling and the end of ADC2 converting, but ADC1 has already  started sampling again by that time so it's not a useful measure of effective sample rate. The delay doesn't affect things here because it doesn't cause a slowdown. ADC1 is ready to sample again immediately after it's done converting.

Calculate the time between ADC1 taking a sample and then ADC1 taking the next sample. That's 2.5 + 8.5. You get two samples during that time (one from ADC1, one from ADC2).

If you increase the delay from 2 to something larger, eventually it starts to affect things. At 4 or more sample rate will slow down. (2.5 + 4 + 2.5 + 4 = 13, which is more than 11)

2 replies

TDK
Super User
June 25, 2025

I calculate 11 cycles (2.5 sample + 8.5 conversion at 8 bit) between readings on the same ADC. The secondary ADC will also convert a channel in this time, sampling delayed by 2 cycles from the master. So that's an average of 5.5 cycles per sample. Not sure how you're calculating 16 cycles here.

At 80 MHz, that's 10.3125 us per 150 samples. Seems to line up with what you're seeing.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Stm325Author
Associate III
June 25, 2025

From the calculation here atthe bottom: Stm32 Interleave 

I calculated as

2.5cycle sample(Adc1) + 2.5 cycle delay + 2.5cycle sample(Adc2) + 8.5 cycle conversion(Adc2) = 16 cycle for 2 samples

Am I doing it wrong? Thanks for the answer and I hope you are right.

 

TDK
TDKBest answer
Super User
June 25, 2025

There are 16 cycles between the start of ADC1 sampling and the end of ADC2 converting, but ADC1 has already  started sampling again by that time so it's not a useful measure of effective sample rate. The delay doesn't affect things here because it doesn't cause a slowdown. ADC1 is ready to sample again immediately after it's done converting.

Calculate the time between ADC1 taking a sample and then ADC1 taking the next sample. That's 2.5 + 8.5. You get two samples during that time (one from ADC1, one from ADC2).

If you increase the delay from 2 to something larger, eventually it starts to affect things. At 4 or more sample rate will slow down. (2.5 + 4 + 2.5 + 4 = 13, which is more than 11)

"If you feel a post has answered your question, please click ""Accept as Solution""."
TDK
Super User
June 28, 2025

Shift the second ADC1 over to the right 1 cycle. It can't sample until it's done converting.

"If you feel a post has answered your question, please click ""Accept as Solution""."