Skip to main content
franz2
Associate III
August 22, 2025
Question

STM32C071 PA14-BOOT0 not working

  • August 22, 2025
  • 3 replies
  • 434 views

Hi
I modified nBOOT_SEL Bit, but still the PA14-BOOT0 Pin level has no effect. The CPU starts always on in Main flash memory. I have these 2 situations (RM0490 Rev 5 page 53)

franz2_0-1755871527351.png

If PA14 is low level: Main flash starts. This is ok
If PA14 has high level: System memory (Internal Bootloader) should start. This is not working. Always application on flash memory starts.
This is the Flash_OPTR content:

franz2_1-1755871742216.png

This is the board schematic:

franz2_2-1755871813785.png

J13 is JTAG: this is working
J12 is access to serial USART loader. RX and TX is connected to PA9/PA10.
J12 serial loader is working in case flash is empty. 
This is the routine for modify the Option Byte:

HAL_StatusTypeDef ClearnBootSel()
{
FLASH_OBProgramInitTypeDef OB;
HAL_FLASHEx_OBGetConfig(&OB);
 
/* OB.USERConfig returns the FLASH_OPTR register */
// Use it to check if OB programming is necessary
if (OB.USERConfig & FLASH_OPTR_nBOOT_SEL)
{

 HAL_FLASH_Unlock();
 HAL_FLASH_OB_Unlock();
 
 OB.OptionType = OPTIONBYTE_USER;
 OB.USERType = OB_USER_NBOOT_SEL;
 OB.USERConfig = OB_BOOT0_FROM_PIN;

 if ( HAL_FLASHEx_OBProgram(&OB) != HAL_OK )
 {
 HAL_FLASH_OB_Lock();
 HAL_FLASH_Lock();
 return HAL_ERROR;
 }

 HAL_FLASH_OB_Launch();

 /* We should not make it past the Launch, so lock
 * flash memory and return an error from function
 */
 HAL_FLASH_OB_Lock();
 HAL_FLASH_Lock();
 return HAL_ERROR;
}
return HAL_OK;
}

Where is the problem?
Thanks for hints.
Franz

3 replies

TDK
Super User
August 22, 2025

Your BOOT0 pin is connected to various things. Perhaps one of these is pulling it low.

The chip itself is likely behaving as described. Option bytes seem set appropriately.

"If you feel a post has answered your question, please click ""Accept as Solution""."
franz2
franz2Author
Associate III
August 22, 2025

I tried also with direct connection of PA14 to GND and to 3.3V. Same issue. And levels are in green range.

franz2
franz2Author
Associate III
August 25, 2025

This is my first project with STM32Cxxx processor. I used in the past 15 years nearly all other STM32 families and I had never this huge problems. It is the first processor I use where Boot 0 is shared with Serial Wire Clock. (Maybe not the best idea)

Problem 1:
Because PA14 is shared with BOOT0 Pin and Serial Wire Clock, we have a new situation in Boot0 reading. If SWD once was active, a reset of CPU will not bring PA14 to his default state: GPIO_IN/BOOT0. Only by removing the full power from CPU will bring back PA14 to his GPIO_IN/BOOT0 state. This was the reason always application was starting up. Because Boot0 was read wrong at startup. 

Problem 2:
When I respect problem 1, I can always make the processor not start up the application. I remove full power. I set Boot0 Pin to high level and reset the uP with a low going impulse on nRST Pin.
Sometimes I can program the uP now, but in 90% of the cases the processor is not answering on his TX Pin (PA9)

franz2_0-1756123726660.png

This is the case serial download is working: blue is the character from Computer. Red is the answer from built in bootloader.

franz2_1-1756123817989.png

This is the case with a download fail. TX Pin (red) is always low, even with Character on RX Pin. So I think internal bootloader is not running or it is running on a wrong interface.

I'll also tried the newest STM32Programmer V2.20.0. Result same failure rate.
I replaced all my cables between STM32C092 board and USB Port of computer. There is no difference. I'm sure there is no failure of cable and electronic. As standard I use FTDI serial to USB converter. But I have same failure rate with a Prolific serial to USB converter.
I use my tools since longer time. I made a bigger 2 digit number of designs with several STM32 uC. And every design, I implement a serial loader with built in bootloader for the mass production line. This C092 is the first project, on which bootloader is not really working with my proofed tools. I plan another design with STM32G071, and this uP has the same sharing of PA14-Boot0 and SWDCLK. Solution is very important.