STM32F303 maximum ADC sampling rate
Hi everyone,
I am currently looking into the STM32F303CCT6 and I'm a bit confused by the ADC specifications. ST's website mentions it can achieve up to 18 MSPS in interleaved mode. However, looking through the Datasheet and the Reference Manual (RM0316), I don't see a clear way to hit 18 MSPS at 12-bit resolution.
I realize the hardware interleaved mode is only dual (e.g., ADC1/2 and ADC3/4). Since the documentation mentions dual mode can reach up to 9 MSPS at 12-bit, and there is no native quad-interleaved mode, I suspect one of two things:
There is a way to manually coordinate the two dual pairs (using all 4 ADCs) to reach 18 MSPS at 12-bit.
The 18 MSPS claim strictly refers to running a dual interleaved setup at a reduced 6-bit resolution.
I would deeple appreciate some insight regarding if 18 MSPS at 12-bit is actually possible on this MCU, or if I am limited to the dual mode specs?
Thanks in advance!