STM32F7xx: SPI CRC Checking Error even when CRC matches
Dear Sirs, we have a SPI CRC problem we thried heavily to solve, but no success.
We broke it down to just send one byte of data, so the CRC is known in advance and it is easy to debug.
Here the description what we did:
Devices
Master: STM32F7 (SPI1)
Slave: STM32F4
Communication mode: SPI full duplex
Data width: 8 bit
CRC enabled on both sides
CRC Configuration
CRC polynomial: 0x07
Data size: 8 bit
MSB first
Only one data byte used for testing
Test frame
Data byte transmitted by slave:
0x55
Expected CRC (CRC-8, polynomial 0x07):
0xAC
SPI clock
The SPI clock on the master is set to the lowest possible speed:
Prescaler = 256
Therefore there should be no timing issue with the CRCNEXT bit being set during the last data frame is clocked.
We use HAL 1.3.3 and HAL_SPI_TransmitReceive_IT on the master side
Observed SPI signals (oscilloscope)
On the SPI bus we observe exactly the expected sequence:
0x55
0xAC
So the slave transmits the correct CRC value.
Master behaviour
When the first SPI interrupt occurs on the master (STM32F7):
A byte is written to the SPI DR register to generate clock.
Immediately afterwards SPI_CR1_CRCNEXT is set.
This causes the CRC phase to start automatically and the slave sends its CRC.
No further write to DR is necessary in this context, because data length is one byte only
Registers on the master after the CRC was clocked in and communication finshed:
CR1
0x0000217C
CR2
0x0000176C
SR
0x00000403
DR
0x0000AC55
RXCRCR
0x000000AC
Interpretation
DR = 0xAC55
The first received byte is 0x55 and the second byte is 0xAC (CRC).RXCRCR = 0xAC
The SPI peripheral calculated the same CRC value internally.SR = 0x403
RXNE = 1
TXE = 1
CRCERR = 1
The SPI peripheral reports a CRC error although:
The CRC value received from the slave is 0xAC.
The internally calculated CRC value (RXCRCR) is also 0xAC.
The SPI bus waveform confirms the transmitted CRC is correct.
Why does the SPI peripheral report a CRC error even though:
the received CRC byte is correct,
the internally calculated CRC value (RXCRCR) matches,
Is there a known condition where CRCERR may still be set although RXCRCR matches the received CRC value?
We also checked the errata sheet of the F7 but nothing appropriate.
Any guidance on the correct sequence for CRC handling in this situation would be appreciated.
Andy