Skip to main content
Associate
July 8, 2025
Solved

STM32G0 ADC Sampling

  • July 8, 2025
  • 4 replies
  • 416 views

Configure STM32G0 to sample 11 channels; When voltage is injected into only one channel each time, the sampling values of all channels are correct. When voltage is injected into 11 channels simultaneously, the sampling values of all channels are incorrect and random values are displayed. Could someone help me explain the reason for this problem and how I should configure it? Thank you.

Best answer by Ozone

> ... and how I should configure it?

You did not reveal much how did you configure the channels right now.
I would not exclude an issue with the code to pick up the ADC results, being it by interrupt/callback or DMA.

Inproper ADC configuration can cause such issues as well.
The input stage, consisting of S&H capacitor and effective input resistance, forms an RC element.
This RC element is consecutively switched to all input channels, charged for the configured time, and then converted.
You need to take care that your input circuitry can charge/discharge this element in the required time.

And besides the actual sampling time (in ADC clock cycles), most STM32 ADC have a configurable delay between consecutive samples.
Try increasing both.

4 replies

mƎALLEm
Technical Moderator
July 8, 2025

Hello, 

It could be due to the output impedance of your voltage source you are measuring.

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
Ozone
OzoneBest answer
Principal
July 8, 2025

> ... and how I should configure it?

You did not reveal much how did you configure the channels right now.
I would not exclude an issue with the code to pick up the ADC results, being it by interrupt/callback or DMA.

Inproper ADC configuration can cause such issues as well.
The input stage, consisting of S&H capacitor and effective input resistance, forms an RC element.
This RC element is consecutively switched to all input channels, charged for the configured time, and then converted.
You need to take care that your input circuitry can charge/discharge this element in the required time.

And besides the actual sampling time (in ADC clock cycles), most STM32 ADC have a configurable delay between consecutive samples.
Try increasing both.

TDK
Super User
July 8, 2025

Probably a bug in the code. There are example projects, I suggest following those. Use DMA to convert multiple channels.

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
Karl Yamashita
Principal
July 8, 2025

Show code, upload your IOC file. 

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source