Skip to main content
Visitor II
September 6, 2025
Question

STM32G0 USBSEL documentation bug?

  • September 6, 2025
  • 1 reply
  • 381 views

Hello, I'm working with a STM32G0B0CE part.  I believe that the TRM definitions for RCC_CCIPR2->USBSEL are incorrect.

I was having trouble with USB, seemingly related to clock selection.  I noticed in the LL HAL headers the following:

#define LL_RCC_USB_CLKSOURCE_HSE RCC_CCIPR2_USBSEL_0 /*!< PLL clock used as USB clock source */
#define LL_RCC_USB_CLKSOURCE_PLL RCC_CCIPR2_USBSEL_1 /*!< PLL clock used as USB clock source */
#define RCC_CCIPR2_USBSEL_Pos (12U)
#define RCC_CCIPR2_USBSEL_Msk (0x3UL << RCC_CCIPR2_USBSEL_Pos) /*!< 0x00003000 */
#define RCC_CCIPR2_USBSEL RCC_CCIPR2_USBSEL_Msk
#define RCC_CCIPR2_USBSEL_0 (0x1UL << RCC_CCIPR2_USBSEL_Pos) /*!< 0x00001000 */
#define RCC_CCIPR2_USBSEL_1 (0x2UL << RCC_CCIPR2_USBSEL_Pos) /*!< 0x00002000 */
 

This seems to indicate that USBSEL should be 0x2 for PLL and 0x1 for HSE.

RM0454 Rev 5 Page 165 indicates that 0x1 is PLL and 0x2 is HSE.

I have confirmed that USB is functional on my board when setting USBSEL to 0x2 and is not functional when using 0x1, so I believe that the HAL definitions are correct and the documentation is wrong.

I'm using an 8 MHz external oscillator and generating a 48MHz output from the PLL, so it is expected that the HSE should not work as a USB clock source.



1 reply

Technical Moderator
September 7, 2025

Hello @DFurie and welcome to the Community,

You are right, the register RCC_CCIPR2 contains incorrect values on the USBSEL field.

An internal ticket (ID: 217013) is submitted to push the update of the reference manual RM0454 with the correct reference :

  • 01: HSE
  • 10: PLLQCLK

Thank you for your contribution and for rising this up.

PS: Ticket (ID: 217013) is only for reference, not available outside of ST.

"When your question is answered, please close this topic by clicking ""Accept as Solution"".ThanksImen"