Skip to main content
Associate II
December 2, 2025
Solved

STM32G4 Half-Duplex Slave early Complete Callback

  • December 2, 2025
  • 4 replies
  • 634 views

Hi, 

I am using STM32G474RE. I try to read out LTC2440 with the SPI interface. I have configured the LTC2440 as SPI master (In its datasheet the mode of operation is specified as Internal SCK, 2-Wire I/O, Continuous Conversion). The LTC2440 provides a BUSY signal which indicates the state of the conversion. LTC2440 does output 4 bytes of data on its own (Burst approx. 880 times / second).

I have configured the SPI interface of my STM32G4 as Half-Duplex slave to read these bursts.

static void MX_SPI3_Init(void)
{
 hspi3.Instance = SPI3;
 hspi3.Init.Mode = SPI_MODE_SLAVE;
 hspi3.Init.Direction = SPI_DIRECTION_1LINE;
 hspi3.Init.DataSize = SPI_DATASIZE_8BIT;
 hspi3.Init.CLKPolarity = SPI_POLARITY_HIGH;
 hspi3.Init.CLKPhase = SPI_PHASE_1EDGE;
 hspi3.Init.NSS = SPI_NSS_SOFT;
 hspi3.Init.FirstBit = SPI_FIRSTBIT_MSB;
 hspi3.Init.TIMode = SPI_TIMODE_DISABLE;
 hspi3.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
 hspi3.Init.CRCPolynomial = 7;
 hspi3.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;
 hspi3.Init.NSSPMode = SPI_NSS_PULSE_DISABLE;
 if (HAL_SPI_Init(&hspi3) != HAL_OK)
 {
 Error_Handler();
 }
}

static void MX_DMA_Init(void)
{
 __HAL_RCC_DMAMUX1_CLK_ENABLE();
 __HAL_RCC_DMA1_CLK_ENABLE();
 HAL_NVIC_SetPriority(DMA1_Channel3_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA1_Channel3_IRQn);
}

 I start the SPI data reception within a callback of the rising edge of BUSY-signal. I disable the "Half-Complete" Interrupt. TIMDBG sets a debug line to HIGH level which we will see on the oscilloscope later. LTC2440_FRAMESIZE is defined as 4. 

void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
	TIMDBG_START;

	HAL_SPI_Receive_DMA(&spi_handle, spi_data, LTC2440_FRAMESIZE);
	__HAL_DMA_DISABLE_IT(&spi_dma_rx_handle, DMA_IT_HT);
}

 For now I have not implemented anything else than a macro, which shows that the conversation has completed. 

void HAL_SPI_RxCpltCallback(SPI_HandleTypeDef *hspi)
{
	TIMDBG_STOP;
}

 
So what I would expect is, that the MCU waits for the rising edge of the BUSY signal. Then it should wait for the data burst from the ADC. After 4 bytes have been received, I should get a callback.However, I get this callback earlier. 

I can observe the following with my scope: 

IMG_20251202_162259.jpg

The first picture shows the clock signal of the burst and the BUSY signal. As expected, BUSY is pulled LOW before the data burst and pushed HIGH after.

IMG_20251202_162228.jpg

The second picture shows the clock signal of the burst and the TIMDBG signal. As expected, the TIMDBG signal is pushed HIGH right after data burst (caused by rising edge of BUSY signal). However TIMDBG doesnt stay high for the entire dataframe, but goes LOW after a few bits. This means, that my receive complete callback is called before receiving the complete package. So I have to assume that my data is corrupted. Why is that? Do you have any troubleshooting tips how I can find the reason for this early callback call? Are thres ome other interrupts I have to exclude? 

P. S.: One might think the observed behaviour might result from the short time between the end of the databurst and the rising edge of the burst signal. I already tried to start the conversation not by the rising edge of the BUSY signal, but by some timer or other ressource. Unfortunately, this didn't had any effect on when my callback routine is called. 

 

Best answer by TDK

Hmm.

The SPI has a 4-byte RXFIFO which may be keeping data and preventing you from resyncing. If it starts out of sync, it will remain that way.

Where you do TIMDBG_START, also read out the contents of the RXFIFO so that it starts from empty when the call happens. Something like this.

spi_handle.Instance->DR;
spi_handle.Instance->DR;
spi_handle.Instance->DR;
spi_handle.Instance->DR;
HAL_SPI_Receive_DMA(&spi_handle, spi_data, LTC2440_FRAMESIZE);

 

4 replies

TDK
Super User
December 2, 2025

We're lacking information on what TIMDBG_START/TIMDBG_STOP is doing. Which one sets it high and which one sets it low?

Looks like TIMDBG_START happens due to EXTI but we are lacking information how this EXTI is configured and what is triggering it.

"If you feel a post has answered your question, please click ""Accept as Solution""."
oeserAuthor
Associate II
December 3, 2025

Sorry for missing information. The macros TIMDBG_START/TIMDBG_STOP are defined as

#define TIMDBG_START HAL_GPIO_WritePin(TIMDBG_GPIO_Port, TIMDBG_Pin, GPIO_PIN_SET)
#define TIMDBG_STOP HAL_GPIO_WritePin(TIMDBG_GPIO_Port, TIMDBG_Pin, GPIO_PIN_RESET)

They just set an unused GPIO pin HIGH or LOW, so that I can see on my scope when the interrupts are happen. 

Yes. TIMDBG_START does happen after an external interrupt. I have configured the pin on the BUSY signal as External Interrupt Mode with Rising edge trigger detection (and Pull-Up enabled).

 

static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};

 __HAL_RCC_GPIOB_CLK_ENABLE();

 HAL_GPIO_WritePin(GPIOB, TIMDBG_Pin, GPIO_PIN_RESET);

 GPIO_InitStruct.Pin = TIMDBG_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

 GPIO_InitStruct.Pin = AFE_BUSY_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
 GPIO_InitStruct.Pull = GPIO_PULLUP;
 HAL_GPIO_Init(AFE_BUSY_GPIO_Port, &GPIO_InitStruct);

 HAL_NVIC_SetPriority(EXTI3_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(EXTI3_IRQn);
}
TDK
TDKBest answer
Super User
December 3, 2025

Hmm.

The SPI has a 4-byte RXFIFO which may be keeping data and preventing you from resyncing. If it starts out of sync, it will remain that way.

Where you do TIMDBG_START, also read out the contents of the RXFIFO so that it starts from empty when the call happens. Something like this.

spi_handle.Instance->DR;
spi_handle.Instance->DR;
spi_handle.Instance->DR;
spi_handle.Instance->DR;
HAL_SPI_Receive_DMA(&spi_handle, spi_data, LTC2440_FRAMESIZE);

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate
December 3, 2025

This early callback usually means the DMA transfer is finishing before the full 4 bytes arrive, which often happens when the SPI slave isn’t fully synchronized with the master’s first clock edges. In half-duplex slave mode on the G4, even small timing differences can cause the DMA to latch initial noise or leftover data. Make sure the SPI is enabled and the DMA buffers are fully ready before the LTC2440 starts clocking. Also check for any leftover data in the RX FIFO and clear it before each burst. Verifying NSS handling, disabling unused interrupts, and comparing your setup with the working SPI example can help narrow down where the premature completion comes from.

oeserAuthor
Associate II
December 8, 2025

Sorry for my late response. I had to work on some other project the last days. However, it turned out, that it helps to read all contents of the RX FIFO as decribed by TDK and darenluie. Thank you very much for your help.